This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50: BMS IC

Part Number: BQ40Z50
Other Parts Discussed in Thread: , BQSTUDIO, EV2400, GPCCHEM, BQ34Z100

Hi TI experts ,

I'm designing a BMS for 3 cells in series, where entire pack is  11.1V and 2500mAH.

I should achieve over voltage protection(12.6v), under voltage protection(9v), over current protection and short circuit protection.

And My charge current should be less than 4A and Discharge current should be less than 8A.

can you please suggest me IC for this requirement and its evaluation Board.

And Do TI BMS chips support parallel connections as well like (3S2P)?

Regards,

Diwakar.B