This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM61460: "Bias" Pin Connection

Part Number: LM61460


Our design has 13.5V/4A Output and Vin=25V

As per Table 6-1 in Datasheet BIAS pin is recommended to connected to ground.


In Webench Design the Bias Pin is connected to Vout.


Do I need to connect this BIAS pin to Vout or Ground for my application?

  • Hi,

    Please connect the BIAS pin to ground since the application output voltage is greater than 12V.

    The image of the WEBENCH design connect looks inaccurate, and I will note this to the team to have it fixed in the future updates. 

    Regards,

    Jimmy