Other Parts Discussed in Thread: TPS65987D, TPS55288, TPS65987, BQ25730, TPS2546
Hello:
We have a cool UCC28782 ac-dc circuit finally fully operational up to 100W , 20V output.
Our intention is to productize it for USBC PD AND a versatile charger.
The base design with UCC28782 shows a WT6636 USB interface chip . We got a fixed ROM based chip from Weltrend.
But now we prefer a programmable approach with full support through a forum such as TI.s
We thus need to find an optimum 1-chip solution to cover the charger/adaptor approach from 5V 3A to 20V @5amp. We intend to make off-USB mark by offering 24V @5amp adaptor/charger.
Our base converter is : exactly as in UC28782EVM specs. But our output will be fixed 24V max 5amp MAX FROM ucc28782 CONTROLLER.
- We can use TPS55288RPMR for all outputs at the receptacle.
- we will have 2 receptacles. One for VBUS PD as a DFP. Another for the charger. If this becomes a necessity.
What we are confused about is the nature of the USB C receptacle: can VBUS output serve as a charger port as well? If so, can the same chip behave as a charger controller through the USB C PD by using configuration signals such as C1/C2 and D+/D- or some other functional pins?
If so, which chip do you suggest we use? I do not think we need any "path selector" or sourcing from an external battery or such capabilities. Our module will be a source only whether for PD or charger. Automatically configuring one or the other.
Is there a chip with such a capability?
Appreciate any clarification on the chip selection.
r