This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596: About feedback resistor

Part Number: LM2596


Hi team,

For LM2596T-12/NOPB,

  • is the internal feedback voltage VFB the same as adjustable version which is 1.23V (1.193-1.267 at Tj=25℃)?
  • What is the tolerance of the internal voltage dividing resistors? Is it 1% for the fixed versions?

Regards,

Ohashi