Other Parts Discussed in Thread: USB2ANY
Hi,
I just obtained a TPS929120EVM evaluation board and its respective GUI. Once I have everything connected and the 12V source connected, a firmware update should pop up. But it doesn't. I tried another computer to see if the problem was that the first one did not detect the USB. But, I still get the same error. If I click to the connect button, it tries to connect but it fails.


What can I do to solve it?
Thanks in advance