This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Minimum duty cycle Ratio for actual lighting

Part Number: TPS92662A-Q1

Hi Experts,

Referring to the datasheet, it appears that a 10BIT RESOLUTION is possible with about 0.1% duty tuning.

In my opinion, it will not turn on when actually tuning 0.1% due to the MLCC effect on the application.

Please check what is the minimum duty that can actually be lit (conditions where FAULT is not detected).

Based on the circuit diagram, both ends of the LED MLCC & GND MLCC: Apply 0.01uF.