Hello,
Q1
My customer is considering to use TPS62700 for the following three cases at Vin=3.3V.
Case#1: Vout=2.7V, Iout<50mA
Case#2: Vout=1.6V, Iout<300mA
Case#3: Vout=1.5 to 2.2V, Iout<200mA
What L values does TI recommend for the above three cases respectively?
Q2
My customer would like to use inductors having less than or equal to 1mm height. Datasheet Table 1 shows Ls having > 1mm height.
Can customer use either of the following Ls?
https://www.murata.com/en-us/products/productdetail?partno=DFE201610E-4R7M%23
https://www.murata.com/ja-jp/products/productdetail?partno=DFE201210U-R24M%23
Best regards,
K.Hirano