Other Parts Discussed in Thread: UCC28781, UCC28782, UCC28C43, LM5155
Hi,
I want to design a multioutput flyback converter with following specifications:
Input : 16 V - 48 V, 28 V Typ
Outputs: 5 V 8 A ; 5 V 5 A ; 15 V 1.5 A ; 15 V 1.5 A ; 28 V 1.5 A
Frequency: 250 KHz
All outputs are isolated
My plan is to control 5 V, 8 A output using input-side switch and some flyback controller IC and for rest outputs use switching regulators. Does that sound good?
I planned to use TL491 as flyback controller but I understand it may not suit at 250 KHz. Please correct me if needed.
My main question is : Can someone please suggest best flyback controller IC for these output and frequency specifications? If Ltspice model and design procedure of this IC is available it is best.