This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: About charging Termination conditions

Guru 21045 points
Part Number: BQ25792


Hi Team,

 

I understand that charging Termination conditons are IBAT and VBAT threshold.

Could you please let us know it if BQ25792 have other monitoring parameters?

 

Regards,

Hide

  • Hi Hide,

    Those are the 2 parameters.  I(BAT) is measured through the BATFET and V(BAT) is measured across BATP and internal GND.  Termination accuracy can be improved by lower the ICHG setting below 1A.  At ICHG < 1A, the charger makes the BATFET more resistive to improve ICHG and ITERM measurements. These measurements are input to comparators and compared against internal references.

    If enabled, the ADC uses the same measurement circuits and converts those analog values to digital but the ADC is not used to perform termination.

    Regards,

    Jeff

  • Hi Jeff-san,

    Thank you for always kind support and the information.

    Regards,

    Hide