This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: BQ34110

Part Number: BQ34110

Hello! t I am designing a device utilizing the BQ34110. I want to use the LiFePO4 battery 12V 20Ah. Meanwhile the datasheet says that "Learn Discharge Current should be large enough so that it generates a cell voltage change of approximately 5 mV or greater. A current level of C/20 or higher is generally recommended." It turns out that Learning load resistor should be big enough to dissipate the power 1A for 10 minutes (More than 1W). Am I correct?