Other Parts Discussed in Thread: UCC37324, BQSTUDIO
Hello,
We are using BQ76952 and are having issues with SCD. When SCD threshold condition is met, the AFE doesn't seem to switch off the DDSG(Discharge FET) FET. The DCHG FET(Charge FET) is switched Off after Short Circuit occurs and never recovers unless the cell connections are removed and plugged in again whereas The DDSG remains on even after Short circuit occurs.
Following are the configurations:
Enabled FET Protections A - 0xBC
CHG FET Protection A - 0x98
DSG FET Protections A - 0xE4
FET options - 0x0D
SCD threshold - 200mV
SCD delay - No delay.
Note: We are using Low-side switching and FETs are in series configuration
Thanks and Regards
Ibrahim Saqib