How long does the gaid command take to execute. Are there any cases in which the tps25750 will fail to execute?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How long does the gaid command take to execute. Are there any cases in which the tps25750 will fail to execute?
Hi Houman,
After sending 'GAID' to TPS25750, the PD controller will immediately goes into the Error Recovery state follow by a 1 second delay (typical) before it does a cold restart. Typically the only reason the 'GAID' command will fail is if the host sends the 4cc command incorrectly to the PD or if the PD does not receive the required power (i.e. 3.3V is cut off to VIN_3V3).
Thanks and Regards,
Raymond Lin