Hello,
If one plans to use the same input voltage on both the PVIN and PVIN_VDD1 inputs (buck 2 and 1, respectively), is it okay to combine the decoupling capacitors and just tie these two pins together? For example, instead of using 1 x 10uF on PVIN_VDD1 and 3 x 10uF on PVIN, just using 4 x 10uF across the input rail and tying both the pins to the resulting rail? Is there concern with the common current paths interacting with one another?
Thanks.