Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6521815: TPS6521815 Input pin deglitch time

Part Number: TPS6521815

Hi, I'm Taka.

I use the PWR_EN pin for power up.

The PWR_EN pin has a deglitch circuit and the deglitch time is typ 10ms.

What is the maximum and minimum deglitch time?

  • Hi Taka, 

    Unfortunately we do not provide a specification for minimum and maximum deglitch time for input signals like PWR_EN as it is not tested in production. This input is intended to be a slow moving signal (high or low for seconds at a time), and the typical deglitch time is a standard value used to filter out any potential glitches on the signal. 

    Best Regards,

    Garrett