This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH12000W: Light load behavior of PTH12000W

Guru 12000 points
Part Number: PTH12000W

Hi,

What happens to the internal switching behavior when the load is less than 100mA, and if the external load goes from light load to normal load, will the switching stop momentarily?

Question background
When the output load of the PTH12000W is gradually increased from a light load state, the output voltage momentarily drops and the output current momentarily becomes a negative value.

Thanks,

Eevee

  • Hi Eevee,

    Is there a pre-bias output voltage existing?
    Is the output of the module connected to other voltages?
    Can you send us the schematic of your HW?
    What is Vin?
    Since this is an open frame module, can you probe the SW node (One side of the inductor) and send us the waveforms when this happens?
    Does this happen on more than a single specific module?

    Under normal conditions, gradual increase of load should not cause this.
    There seems to be something specific about your application that triggers this behavior.

    Regards,

    Yitzhak Bolurian

  • Hi, Yitzhak Bolurian

    I would like to provide circuit diagrams, etc., but it is confidential information. Would it be possible for you to close this thread and send us a private message.

    Thanks,

    Eevee

  • Hi Eevee,

    Yes, please sent me an email.

    Regards,

    Yitzhak