Dear members,
we have used LM25085 to control a FAN by changing the duty cycle. I want that this circuit limits the current at 4A. Input voltage will be 0 to 12V according to duty cycle.
Rsense= 0.030 ohm. Having 30mOhm I observed that with maximum duty cylce it limits the current at 2.3A. I reduced the Rsense to 22mOhm and 15mOhm but nothing changed. I know that the FET also has an internal R that may affect the limiting. reducing the Rsense, I didnt get a correct result.
I will appreciate any suggestion
Thanks
Farzaneh