I bought a BQ3060EVM and some BQ3060 ICs. The EVM works fine. So i tried to replace another BQ3060 IC with the EVM to test the IC. i assumed that it has a default setting like the BQ3060 that came with the EVM and other 20zXX, but the bqEVSW doesn't recognize the IC and i couldn't read from the SBS or the data flash. Please let me know if there is a certain steps that i have to follow to initialize the IC or write the default data to it. I place the BQ3060 that came with the EVM back and it works fine again.
Frank