Hello everyone
If been using the TI TPS61021A Boost converter to drive an LED with Vin=1.5V
Im trying to boost the 1.5V to 3.6V with Iout=1A
I have done a hardware test setup and without load I have the 3.6V that I want. When I connect a load, I do not get more Output current then 250mA.
Can someone answer me, why I cant get Iout=1A?
My schematic:

LED: Vf=3V @ 600mA
Thank you so much for your help!