Part Number: UC3854
Other Parts Discussed in Thread: UC1854, UCC28070, UCC28180, UCC28019, UC2854
I started designing with the UC3854, but found that the operating temperature rangetemperature condition of 0-70°C is NG.
From the product specifications, I think that 100°C or more is necessary, but UC1854 is too high cost.
Also, I have experience using the UCC28070 with a single-phase input, but when the rectified voltage of the input is disturbed,
since the operation became unstable, we would like to consider another part number.
I will present the specifications bellow, so please tell me the recommended PFC controller candidates.
- Input : AC200V to 240V (three-phase three-wire system)
- Output : DC390V 1800W-4000W
- Environmental temperature : 0°C to 70°C (The controller rating should be 100°C or higher considering heat generation due to loss.)
- Signal : Output OV, Output UV, Output OC (Use an external circuit if there is no function)
- Others : Parallel operation 1 to 3 units