Part Number: TPS55340
Hello,
I was wondering if this design really works as it is proposed by the WEBENCH Power Designer. I am concerned that it is not possible to unload the inductor completely with that switching frequency and high duty cycle and also I am wondering if the switch current is calculated correctly and still within the maximum possible ratings for this device. The Input is a 3V Source and the Output is 35V @ 0,3A.
4150.WBDesign62.pdf
Please Help.

Here again in better Quality: https://ibb.co/zSj52hD