Hi team,
What will happen if customer leave LM3481-Q1 pin FA/SYNC/SD floating? Can IC operates at certain fix frequency or it cannot work normally? Thanks
Scarlett
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
What will happen if customer leave LM3481-Q1 pin FA/SYNC/SD floating? Can IC operates at certain fix frequency or it cannot work normally? Thanks
Scarlett
Hi Scarlett,
Thank you for using E2E forums, regarding your query this pin is needed for adjusting the frequency adjusting and that seems to be necessary for it to be fixed at a single frequency through a resistor. how will it fix at a frequency if the pin is floating?
BR,
Haroon
Hi Haroon,
Customer would like to know if the pin can be left floating. It is not recommended, or it can be used by frequency not stable? Thanks
Scarlett
Hi Scarlett,
Thank you for your reply, This is pin is not supposed to be left floating. When tested on the EVM the voltage level is 0.94V, so it is not supposed to be left floating.
BR,
Haroon
Hello Scarlett,
I have not seen an update from you for the last 24 days, so I assume the questions are answered and the issue is solved.
I close this thread now. If there is still something open, please reply and the thread will get opened again.
If you have any other question or of the thread has been locked, please open a new one.
Clicking the Resolved Button also helps us to maintain this forum.
Best regards,
Harry