Hello team,
I received a question from the customer.
Does Output Accuracy have the following?
-Error in Internal reference (0.641~0.659)
Error in Load regulation (0.33)
The internal reference is listed as 0.641 - 0.65 - 0.659 [V] and reads 0.65V ± 1.38%. If they have to be considered individually, the VREF error ± 1.38% and Output Accuracy ± 1.5% would add up to a worst-case output error of nearly ±3%.
Regards,
Masa