Hello E2E Experts,
Good day.
Thank you in advance for your assistance.
Regards,
CSC
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E Experts,
Good day.
Thank you in advance for your assistance.
Regards,
CSC
Hello Given,
Thank you for reaching out.
0.7 V would be the voltage drop due to the high side FET and the inductor. If you operate the device beyond that condition it could enter into 100% Duty cycle mode.
Thank You,
BR,
Moheddin
Hello Moheddin,
Good day.
Just one follow-up, for TPS62742, what will happen if we run the 300mA for 100mS pulses at a 1sec period when it’s in 100% duty cycle mode?
Regards,
CSC
Hello CSC,
Can you please provide me your test conditions such as Vin, Vout and Iout. Because the device enters into 100% duty cycle mode based upon the your Vin, Vout and Iout.
what will happen if we run the 300mA for 100mS pulses at a 1sec period when it’s in 100% duty cycle mode?
Lets imagine that the device is in 100% duty cycle mode, then the high side FET is always ON and the Vout follows the Vin with reduction in voltage drop due to Rds ON of high side FET and inductor DCR. Now if there is a load transient condition, the device jumps form 100% duty cycle mode to switching mode based upon the load transient current.
if we run the 300mA for 100mS pulses at a 1sec period
Can you please elaborate the condition.
Thank you,
Regards,
Moheddin.
Hello Moheddin,
Good day.
Our test condition:
Vin = 3.3
Vout = 3.0
Iout is dynamic based on the wireless SoC.
Pls, see attached. This is a typical current consumption profile on 3.3V rail during 10 second period consumed by the TI CC3235 module we have.
Attachments.zip
You can see there are periodic WiFi activities that peak up to more than 150mA, but most of the time is much less than 100mA. It can be as high as 300mA for 100mS for each 1-second period.
What is the risk of using TPS62742?
Regards,
CSC
Hello CSC,
I will get back to you by end of the day.
Thank you,
Regards,
Moheddin.
Hello CSC,
The 400mA maximum current defined in the datasheet is the sum of ILOAD and IOUT. So the maximum IOUT for TPS62742 is 300mA.
I assume you are using only the IOUT for output. In this case your load is exceeding the maximum load conditions.
I see the maximum load of 413.21mA in the attachment you shared. If your load is around 300mA with transient then you can go with TPS62742.
I would recommend our new device TPS628438 which is having smaller Iq of 275nA and also 600mA load capability available in WCSP package. (TPS62843 data sheet, product information and support | TI.com)
You can also check our lowest Iq device TPS6284X- (TPS62840 data sheet, product information and support | TI.com)
If you have any further questions please feel free to contact.
Thank you,
Regards,
Moheddin.
Hello CSC,
If you don't have any further questions, can you please close the thread by clicking on Resolved.
Thank you,
Regards,
Moheddin.