This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170EVM-BIDIR: LM5170-EVM-BIDIR-EVM BIAS SUPPLY and R4

Part Number: LM5170EVM-BIDIR

Hello

I have a confusion regarding startup of EVM board, I am working on boost mode 24/48. I want to run the board first without installing the R4 resistor, so do I be able to start the board with only external 3.3V supply at J17 PIN5? AND I want to use the on-board 10V AUX supply, so am I be able to use that supply without R4? Because as per my understanding R4 resistor pulls up UVLO to start the board if voltage supply is given at LV 12V port.

Thanks