Hello.
Please tell me, is it possible to use zener diodes to protect the gates MOSFETs as shown in the figure (red circles)?
I have doubts that when the VT5 transistor is closed, at a battery voltage of, for example, 16.8V, a current of approximately 3mA will flow through the VDZ20 -> R20 circuit,
which will increase the self-discharge of the battery. Moreover, when the transistor VT7 is closed, with a large voltage surge from the side of the charger, too much current
may flow through the VDZ21-> R27 circuit, which will damage the microcircuit.
In addition, is it possible to use a bidirectional TVS diode VDZ10 (blue circle) at the battery output, or should I use a unidirectional one?