Hello.
Please tell me, is it possible to use zener diodes to protect the gates of MOSFETs as shown in the figure (red circles)?
I have doubts that with closed transistors VT12 and VT13, with a large voltage surge from the side of the charger or load,
too much current may flow through the VDZ12 -> R89 circuit, which will damage the driver chip.
Is it possible to install a zener diode to protect the gates of charging MOSFETs (a bunch of VDZx and Rb in the figure)?
I have doubts that with transistors VT9 and VT10 closed, current will flow through the VDZx -> Rb circuit, which will increase
the self-discharge of the battery.
And is it possible to use a bidirectional TVS diode (VDZ16) at the battery output, , or should I use a unidirectional one?