Other Parts Discussed in Thread: TINA-TI
Hello,
I am using UCC28701 to design a flyback converter. And I am a little confused by the system operating frequency.
I see the following figure from the datasheet. Is VCL the same as the voltage sampled at VS pin?
If yes, the voltage at my VS pin reaches around 4V and based on the figure the fsw should be around 80kHz.
But the simulated frequency in TINA-TI Spice is much lower than what shows in the figure (only around 20kHz).
Could any one help clear my confusion? Will my hardware operating at 20kHz as the software shows?
The TINA-TI Spice file is also attached. Thanks.