This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Buck Converter IC with Multiple Outputs

Hello Sir,

Input Voltage: 24V DC
We are looking Single IC (Buck Converter), Which will generate Multiple Outputs as below
Output 1 : 1.2V @ 500 mA
Output 2 : 2.8V @ 300 mA
Output 3 : 1.8V @ 500 mA

Please Suggest Single IC & separate ICs for the above requirement.

Regards
Murthy