Other Parts Discussed in Thread: UCC28730, PMP
Hi, TI support team
The UCC28730-Q1 product is referring to the circuit configured as below.
Please advise which part needs to be changed or modified to configure the circuit under the conditions below.
Input Voltage(Battery) : 100~130V
Output Voltage/Current : 24V/3A
Thanks.
Regards,
MJ