Hi,
I am designing for a GSM/GPRS application.Here the Digital load(uC and Modem etc) can take upto 4.0 Volts(absolute Max) and 3.3V recommended.
I am planning to use bq24070 as a charger and give its Vout to my digital load.
I am planning for Li-ion Single cell 3.6V ,950 mAH Battery.
The Adapter gives 5.0 V DC.
In Case of Adapter Present, can the bq24070 regulate the DC to 3.3 Vout?
When the charger will cutoff the battery ?2.65V?Will it try to boost this voltage on Vout?
Do you recommend any Buck-boost after the Charger my load current and voltage requirement is 3.3V ,2.2A?