dear
I want use LM5158 to output +/- 75V/25mA voltage from a input voltage 3.0V~5V. for evaluation the design, I do some simulation and try to evaluate the performance. however, the simulation is always slowly and stop simulation than I configured. is there any one in product line help to find root cause? thanks.
regards,
Bill