Other Parts Discussed in Thread: LMR54406, LMR43620
Hi all
My customer has a design with the LMR50410 with these specs:
Vin= 22.8V ... 25.2V
Vout = 5V to 0.98*Vin (PWM controlled on FB Pin via a summation node)
Iout = 0.1 to 0.4 A
And they have this question:
Does the LMR50410XFDB (fixed 700kHz frequency variant) also have the frequency foldback for high duty cycle of 98% (133kHz) ?
Other comments on the above spec are also appreciated.
Best regards
Ueli