Part Number: BQ76952EVM
Other Parts Discussed in Thread: BQ76952
Hi Team,
Can you please help us with this inquiry from our customer?
What is maximum Ampere output of EVM board?
I plan to accurately measure current on various boards without limiting the output current. Because my system(motor) needs like 100 Ampere. so I planned to use the below structure.

This card will measure the current passing through the main board, and will protect the system through a fuse if the current exceeds a certain level. The switch on the board will allow for disconnecting the output of the main board. the shunt resistor is going to be on current board and it will connect directly to my main board over pins (headers).
Do you think this structure can work to measure all the current that i use ? i hope that i made my question clearly.
Regards,
Danilo