This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28810: Suitable for 230V/9A application?

Part Number: UCC28810

Dear all,

I need to design a sepic converter with PFC and the following specifications. Vin 85VAC - 265VAC, Vout 230VDC, Iout 9A.

I am now unsure if i can use the UCC28810 for this application. Or could you propose an other IC for this?

i can find a lot of controllers for Sepic topologies, but the PFC is a must that I need to have implemented.

Thanks in advance for any help.