Hi,
Please kindly review below silk-screen, and our customer consider the second line is different, and the IQC deperatment has some query, thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Please kindly review below silk-screen, and our customer consider the second line is different, and the IQC deperatment has some query, thanks.
Hi Liang,
Please refer to below information.
So it's clear that the second line is the date. The last line is the assembly lot or site code which doesn't make function a difference.
Hi, Ziv,
Our customer IQC consider the two device have many different for the prints, and they wants to know if there are any offical file to explain,
Please kindly provide the below difference result:
1. Why the Pin#1 is the line in the pirture 1 and the spot in pirture;
2. Why the "TI letters" on pirture 1 and pirture 2 are different icon;
3. 12 is mean Feb. 2021 in pirture 1, and 2C is mean Dec. 2022, right?
So please also kindly check if there are any PCN file to provide, thanks.
Hi Liang,
Have a check of the part number you offered.
See below information:
So the only different is assembly site.