This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: INT_LDO3_4 Register I read the bit (LDO4_SC_INT) is 1,what is the meaning of it?

Part Number: TPS6594-Q1

Hi,

    We read the register  of TPS65941212RWERQ1 via IIC, found the LDO4_SC_INT  is 1,we write this register to clear this bit ,but not success.

we test the voltage of LDO4 1.8V, and the system works properly.

datasheet describe the meaning of this bit ,but I do not understand. it mean the voltage ripple is high or not ?