Hello team,
I simulated TPS562211 for Vin=12V, Vout=3.3V, Iout= 0.5A
Accordingly, I changed the inductor value which is calculated using Equation 12 for Lmin(circuit is attached for reference).
So Lmin=15.95uH which is approx 16uH. After simulating it for above values, I got results as attached below. It is not getting simulated properly.
Whereas, for 4.7uH, the circuit is working properly for same load and I am getting correct results.
So, will the circuit work or not for selected value of inductor?
Thanks,
Siddhi