This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28600: Examination of isolated power supply

Part Number: UCC28600


Hello,

I am an FAE for a distributor that handles TI products.
My customer is considering the following specifications.
I think the UCC28600 device is applicable, but are there any other good devices?
Also, if you have a reference design, please provide it to me.

(specification)
Insulation required
VIN=390V (PFC output)
VOUT=5V
IOUT=18A (steady state), 24A (peak)
Efficiency: about 92%
Environmental temperature: 60℃

Best regards,