This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90120A: Override pre-programmed power sequencing during run time

Part Number: UCD90120A

Hi Sir,

The power on/off sequence of our product is configured by TI's GUI tool and programm into UCD

In some case we want to modify the behavior of one of power rail enable to force it on even previous power rail is non-available via PMBus command without modifying UCD image.

Is it possible? and how to do it?

Another question: we just check the GPO_CONFIG(F8h) setup via PMBus command, but can't find and related setup with the pre-programmed image.

For example, here we configured P1V8(Rail#8) is one of the input source of the AND gate, but the reading output of GPO_CONFIG(F8h) is "15 3e 86 00 00 00 00 04 00 00 00 00 00 00 00 00"

Except the PAGE configuration, is there anything I need to setup before accessing?

Thanks,
Jim