This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61500: Unique LED driver Vf:3V Imax:3A

Part Number: TPS61500
Other Parts Discussed in Thread: LM3409

Hi,

I'm looking for an efficient solution (>90%) to drive a unique led(Vf:3V Imax:3A) from 8V to 16V input with a PWM dimming input.

I've found the TPS61500 , is it suitable for my application ?

Is there a solution with a smaller component ?

Thanks for your help