This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: why input current limit is 3.3A only ?

Part Number: BQ25792
Other Parts Discussed in Thread: BQ25720

Hi team,

BQ25792 input current is 3.3A, so is this means when customer used 4s battery with 16.8V max battery voltage can't get 5A charge current?

assume input voltage is 20V, battery is 4s with max voltage 16.8V, charging efficiency is 90%, then the input current need 16.8V*5A/0.9/20V=4.7A, obvious exceed the input current limit.

Thanks.

Anderson