Other Parts Discussed in Thread: UCC27614, LM5112
Hi Experts,
Could you propose a driver to send pulses from FPGA (3V3) to cable with a 50 Ohm load?
I found some line drivers, for example, UCC27322, but I'm not sure that this is the optimal component for a task.
Cable capasitance up to 1nF
Single pulses length 500ns
Pulse amplitude 2.4V...5V (the load 1nF, 50 Ohm)
rise time & fall time <=50ns (the load 1nF, 50 Ohm)
Driver's V input high <= 3,3V (FPGA output)
Driver's Vcc - preferably 3V3 or 5V
Channels 1 (maybe 2)
Thank you in advance for your support.
Best regards,
Jonathan