Other Parts Discussed in Thread: TPS548B27
It appears that our TI power supplies appear to be unstable. When I run the TI Webench, it complains about the low divider resistance in the feedback path, but the data sheet recommends starting with 1mA of current through R1. This yields a low resistance of 1.21 kΩ. It seems to accept the changes once I have updated both R1 & R2 to their 1.40K and 2.45K values.
According to TI Webench, the following circuit should achieve:
- Phase Margin = 59.81°
- Crossover Frequency = 49.66 kHz
- Gain Margin = -13.97 dB
- Switching Frequency = 403.13 kHz
From the data sheet, it states that the compensation network should be selected at least an order of magnitude less than the target crossover frequency. In this case, we would want the compensation network to yield a desired compensation network zero of 4.966 kHz. Currently the zero is at 6.412 kHz.
But from my measurements with a Network Analyzer, this is what I see:
This reports the following:
- Phase Margin = 27.792.81°
- Crossover Frequency = 47.850955 kHz
What is wrong with the circuit above that is causing such results?
Regards,
Jeff K