This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700EVM-139: Heat traps to plane

Part Number: TPS63700EVM-139


Hello,

Our customer plan an 8-layer PCB including two ground planes and two supply planes. While our evaluation board TPS63700-139 is implemented with a two-layer PCB,
they are asking if they can use heat-traps ("cross-hair") for the power vias or does that give too much inductance for the TPS53700 ground pad and input and output capacitors?
Vin = 5 V, Vout = -5 V, and Iout = max.

Thanks in advance.

Art