We are having some problems related to electrical consumption of an equipment project that uses a 9V alkaline battery, and we noticed that the input capacitors on pin 2 Vi are below the specified in the datasheet (20uF), due to batch variation or tolerance, my question is the following, at least the fact that they are out of specification, this can cause a problem that can impact the consumption of the equipment when turned off, or somehow damage the Ci (TPS63060)?
Thanks