This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23753A: Schematic check

Guru 11170 points
Part Number: TPS23753A


Hello E2E,

Our customer is evaluating their designed board using the TPS23753A for PoE. This system output voltage setted 5V.
I was conserned from customer that the output of the board has vibration when input 12-V DC and output current over 0.77-A.
I received that schematic, but I could not pick up cause point.

Could you check the schematic? If it's OK, I send it on private message.

Best regards,
ACGUY