Other Parts Discussed in Thread: BQSTUDIO
As the title states, I am currently trying to calibrate the BQ76952 through the BQStudiio Software, however cell 10 is not being calibrated correctly. (Cell 10/VC16 reads 2.7 V instead of 3.1 V on pack 1, and 3.15V instead of 2.8 V on pack 2)
Cells 1-9/ VC0-10, stack and pack voltages all calibrate through the calibration tool in BQStudio, reasonably accurately. It is just VC16 that has problems. We are using 20 Ohm resistors with 220 nF for all cell tap measurements (just like the reference design)
Any suggestions about how to get the top cell to calibrate correctly as this is obviously going to cause us problems moving problems if we can not calibrate the top cell correctly.
Any questions please ask, and I will provide as much information as I can.