Other Parts Discussed in Thread: TPS65987, BQ40Z50
I am looking for a USB-C PD Device that will respond correctly to the command from section 9.3 "PD Specific Requests and Events", Extended Message, (0 0100 Get_Battery_Status Source or Sink See Section 6.5.4)
Is there any way of implementing this in off the shelf devices such as the: TPS25750 or the TPS65987. This information would need to be placed into EEPROM at the correct location so it can be returned on command from the CC Line.
(From Universal Serial Bus Power Delivery Specification Rev3.1)