This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

We currently want to choose a driver

We currently want to choose a driver, mainly used to drive UV lamps, input 5V DC, boost output AC1000V or so to excite UV UV lamps, power 2W, this design has high requirements for PCB layout, so it requires enough peripheral devices, preferably built-in Mos, the package should be small enough, is there a suitable recommendation?