This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: BQ40Z80 RSOC drop when use LiFePO4

Part Number: BQ40Z80
Other Parts Discussed in Thread: GPCCHEM

Hi

The customer mass production with BQ40Z80, The cell is LiFePO4. The problem is RSOC will drop from 100% to 69% - 73% after 5 hours placement.

If set LFP_RELAX=1, Whether RSOC jump problem can be improved.

Waiting for your reply.

Thanks

Star